Wiring - Metasys - Part No. 24-11064-00048 - DX-FAC-Adapter - Field Device - DX-FAC-Adapter

DX-ADPT-FAC4911 Installation Guide

Product
Accessories > Adapters > DX-FAC-Adapter
Document number
Part No. 24-11064-00048
Document revision
A
Revision date
2021-06-18
Part number
24-11064-00048

Most connections come pre-terminated through the use of the wiring harnesses.

Communication wiring must be terminated directly to the FAC . Power input wiring is required for the FAC in addition to the existing power input wiring used for the base of the DX controller.

Figure 1. Wiring connections

The replacement controller has fewer I/O terminal points than the original DX controller.

Note: For most applications, you may use the existing DX mounting base terminal blocks as a termination point for jumper wiring to bring these extra points to IOM modules.