Features and benefits - Metasys - LIT-1901142 - DX-ADPT-FAC4911 - Field Device - DX-ADPT-FAC4911

DX-ADPT-FAC4911 Catalog Page

Brand
Metasys
Product name
DX-ADPT-FAC4911
Document type
Catalog Page
Document number
LIT-1901142
Part number
Revision date
2020-07-10
Language
English
Uses existing base of the DX Controller
Allows the footprint mounting location of the replacement FAC4911 to remain the same as the existing DX-9100 Series controller. The addition of a new panel to meet the physical requirements of the FAC4911 may be avoided.
Field Wiring terminated to the base of the DX Controller
Requires minimal re-wiring because the base is reused and is not removed from the panel. The DX-ADPT- FAC4911 comes with most terminations pre-wired and ready to be assembled. Test sites determined that this feature alone could save hours of field labor time for each controller upgrade.
Pre-wired to the FAC4911 Controller
Reduces or eliminates the chance of wire termination errors.