Procedure
- In the DLLR object, click the Load Summary tab. The Load Summary view appears.
- Click the Setup radio button.
- Click Edit.
-
To edit a single load, edit the attributes for the load and go to Step 7.
To edit multiple loads, select the loads you want to edit and click the MultiEdit button. Select multiple rows using Ctrl and Shift. The MultiEdit dialog box appears (Figure 1).
Note: The button is not enabled until you select more than one load.Figure 1. MultiEdit Dialog
- Enter new values for the load properties. If you do not want to change a value, leave it as 0.
- Click OK. The values update in the Load Summary.
- Click Save.
Related reference