Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15
About this task
For details on using the Load Summary - Runtime view to monitor DLLR, see Load Summary - Runtime.
Procedure
Open the DLLR object.
Click the Load Summary tab. The Load Summary - Runtime view appears.
Note: The Load Summary - Runtime view is the default view and the view used for
monitoring purposes. Select the Setup radio button to add or remove loads.
See Creating the DLLR Object.