Deleting Loads - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

Procedure

  1. In the DLLR object, click the Load Summary tab. The Load Summary view appears.
  2. Click the Setup radio button.
  3. Click Edit.
  4. Select the load you want to delete and click the Remove Load(s) button. You can select multiple rows using Ctrl and Shift.
  5. In the output object, click the Load tab. The Load extension appears.
  6. In the Select Item(s) box, select the load you want to delete.
  7. Click the Delete button.