Commanding a Load Extension - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

About this task

For details on commands, see DLLR Commands.

Procedure

  1. Open the DLLR object.
  2. Click the Load Summary tab. The Load Summary - Runtime view appears.
  3. Right-click a load and select Load Commands.

    The Load Commands selection box appears (Figure 1).

    Figure 1. Command Options for a Load Extension

  4. Select the command you want to use. For a description of all commands, refer to Metasys System Help (LIT-1201793).
  5. Click Send to issue the command.