Commanding a DLLR Object - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

About this task

For details on commands, see DLLR Commands. For details on selecting modes, see Setting DLLR to Shed Mode.

Procedure

  1. In the navigation tree, right-click the DLLR object and select commands from the box that appears (Figure 1).
    The DLLR object Commands selection box appears (Figure 2).
  2. Select the command you want to use. For a description of all commands, refer to Metasys System Help (LIT-1201793).
    Important: Under normal circumstances, the Reset Initialization Parameters command should not be issued while DLLR is in Shed mode. This may disrupt a smoothly operating DLLR feature by forcing it to reinitialize. To prevent an operator from accidentally issuing this command while in Shed mode, the Reset Initialization Parameters command is not permitted in Shed mode while the Allow Reset in Shed Mode attribute is set to False. An authorized operator may change this attribute to True, which would allow the Reset Initialization Parameters command to be issued when in Shed mode.
  3. Click Send to issue the command.