About this task
Note: You also can perform this task by editing the Mode attribute in the DLLR Focus view.
Procedure
-
Once you are satisfied with the DLLR configuration, in the navigation tree,
right-click the DLLR object and select Commands from the box that appears (Figure 1).
Figure 1. Command Selection Box
The DLLR object Commands selection box appears (Figure 2).Figure 2. Command Options for a DLLR Object
- Click Set Mode.
- From the drop-down list box, select Shed.
- Click Send to issue the command.
- Open the DLLR object.
- Click the Load Summary tab. The Load Summary - Runtime view appears.
- Monitor which loads are being shed.
- Make changes as necessary.