Adding Load Extensions to Output Objects Eligible for Load Shedding - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

About this task

You can define only one Load extension per object. See Chiller/Boiler Step Strategy for an example of an application with logic needed to work around this restriction.

For more information on eligibility, see Load Eligibility.

To add Load extensions to output objects eligible for load shedding:

Procedure

  1. Select the output object in the navigation tree.
  2. From the Action menu, select Show Extensions. Alternatively, right-click and select Show Extensions.
  3. Click the New button to add a Load extension.
  4. Complete the information in the Insert Load Wizard. For descriptions of Load extension attributes, refer to Metasys System Help (LIT-1201793).
  5. Click Finish on the Summary page to create the Load extension.
    Note: In SCT, you can copy and paste Load extensions.
  6. If you are using a DL strategy, go to Creating a Meter Object (DL Strategy Only). Otherwise, go to Creating the DLLR Object.