Configuring DLLR - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

About this task

You can perform these steps offline or online. If you define the DLLR feature offline with SCT, you can easily copy and paste Load extensions of the same type with SCT. If you are defining the DLLR feature online, use the Site Director because it has access to the DLLR and meter objects and all loads from different engines.

To configure the DLLR feature, see the following sections in order:

Procedure

  1. Adding Load Extensions to Output Objects Eligible for Load Shedding
  2. Creating a Meter Object (DL Strategy Only)
  3. Creating the DLLR Object
  4. Associating Loads to the DLLR Object
  5. Verifying DLLR Operation
  6. Setting DLLR to Shed Mode