Load Eligibility - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

A load is not eligible to be shed by DLLR if:

  • the load is disabled or locked

  • the load is already shed

  • the load has a Comfort Override command in effect

  • the minimum release time has not expired

  • the load output is offline, unreliable, or out of service

  • the load output is controlled by a higher priority command

  • the load output has a value that does not permit shedding (for example, a Supply Fan command load that is already commanded Off)

  • the output minimum on-time has not expired

  • the Load extension Alarm Reference for Ineligibility attribute is in alarm