Load Deletion - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

To delete a load, you first must remove the load from the DLLR object Load Summary - Setup view, then delete the Load extension from the output object. If you delete the Load extension without first removing the load from the DLLR Load Summary - Setup view, the load appears grayed out in the Load Summary; however, you can still remove it from the Load Summary.