To help monitor DLLR operations, we recommend that you trend important DLLR object attributes and place the trended values in a Trend Study. Attributes that you may want to trend include: Amount Shed, Energy Rate, Interval Demand, Uncontrolled Interval Demand, and Active Demand Limit. The Trend tab appears on the DLLR object after you create the trend extension.
Figure 1 is an example of a Trend Study. For details on how to trend values and add them to a Trend Study, refer to Metasys System Help (LIT-1201793).
Figure 1. DLLR Trend Study Example