Load Summary - Setup - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

To view the Load Summary - Setup view, click the Setup radio button. Setup allows you to define DLLR by adding and removing loads associated with the DLLR object. Figure 1 is an example of the Setup view.

Figure 1. DLLR Load Summary View - Setup

For a description of all attributes, refer to Metasys System Help (LIT-1201793).