Load Summary View - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

The Load Summary view appears when you click the Load Summary tab on the DLLR object. The Load Summary contains information related to every load associated with the DLLR object.

You can view either the Load Summary - Runtime view or Load Summary - Setup view. See Load Summary - Runtime and Load Summary - Setup.

Note: The Load Summary view is not visible if you are using SCT Simulation.

For a description of all attributes, refer to Metasys System Help (LIT-1201793).