DLLR Monitoring - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document type
Technical Bulletin
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

You can monitor the daily operation of the DLLR feature using the DLLR object tabs: Focus, Profile, and Load Summary. The Focus view contains the overall operation of the object, the Profile view lists energy consumption and peak energy values for the current and previous tracking period, and the Load Summary view is a table showing the status of the loads and which loads are being shed and/or released.

You also may find it helpful to create a Trend extension on the DLLR object and a Trend Study to monitor the trended values of important DLLR object attributes, such as Amount Shed, Current Demand Limit, Interval Demand, Uncontrolled Interval Demand, and Energy Rate. For an example, see Trend Extension and Trend Study.