Each output object that you intend for DLLR control must be added to the Metasys software as a Metasys field point or object. Two object tabs are of special importance to DLLR: Options and Load.
The Options tab contains the Options view (Figure 1). If the output object is not from a controller on a BACnet® MS/TP field bus, select the Demand Limiting and Loading Rolling check boxes under the Restart Options section. This ensures that the load releases if the device is reset. Also, if this is an N1 Analog Output point, specify a restore value in the Relinquish Default field and set the Ignore Relinquish Default attribute to False.
The Load tab contains information configured when you define the Load extension for the output object. See Load Extension.
Refer to the Metasys System Help (LIT-1201793) for details on output object attributes.