Each object that is defined as an output for use with DLLR requires a unique Load extension. After you create a Load extension, a Load tab appears for the output object. The Load tab contains the Load view (Figure 1).
Typically, you add a Load extension when the object is created, but you can add one at any time. Objects with Load extensions have a Load tab. Clicking the Load tab displays the Load extension attributes that tell DLLR how the object can be controlled. Only one Load extension is allowed per object, which prevents the possibility of two Loads trying to control the same output at the same time.
Note: See Chiller/Boiler Step Strategy for an example
of an application with logic needed to work around the restriction of one Load extension
per object.
Figure 1. Load Extension for an Object

Refer to the Metasys System Help (LIT-1201793) for details on Load extension attributes.