After you define the output object, Load extension, and meter object, you must define the DLLR object. Figure 1 shows an example of a DLLR object.
Figure 1. DLLR Object Focus View

The tabs used for DLLR object definition are the Focus tab and the Load Summary tab (Setup view). These tabs, along with the Profile tab, Load Summary (Runtime view) tab, and optional Trend tab also are used in monitoring DLLR. See DLLR Monitoring.
Refer to the Metasys System Help (LIT-1201793) for details on DLLR object attributes.