Fixed Window Algorithm - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

The Fixed Window algorithm is used if the energy utility billing interval starts at the end of the previous interval with no overlap of data from the previous interval. This algorithm typically uses an EOI pulse, supplied by the utility company. The EOI pulse is used to synchronize the DLLR demand interval to the utility demand interval.

For details on the attributes and advanced attributes that contribute to the Fixed Window algorithm logic, refer to the Metasys System Help (LIT-1201793).