Potential Load Candidates - Metasys - LIT-12011288 - Software Application - Metasys Building Automation System - 6

DLLR Technical Bulletin

Product
Building Automation Systems > Building Automation Systems > Metasys Building Automation System
Document number
LIT-12011288
Version
6
Revision date
2013-10-15

Based on the target information, determine the following:

  • Which loads can be considered for shedding?

  • Is scheduling or some triggering process needed to limit the availability of the load as a shed candidate?

  • Which priority is appropriate for each load?

If you use DLLR to control loads on an NCM that is part of an N1 integration:

  • Do not allow any Metasys preventive maintenance and inspection (PMI) feature, such as scheduling or the Graphic Programming Language (GPL), to control the loads. For DLLR to control the loads properly, all controlling features must be part of the Metasys System extended architecture.

  • Make sure that any Shed and/or Release commands do not persist if the NCM that contains the loads loses power.