The Load extension and DLLR object can be commanded, subject to user credentials in the Metasys system. Commands for the Load extension include manual load shed/release, overrides, locks, and others. Commands for the DLLR object include mode selection, profile/interval/parameter resets, and others. Refer to the Metasys System Help (LIT-1201793) for details on Load extension and DLLR object commands.
Consistent with other Metasys system features, all attributes that you can command also may be scheduled with the Scheduling feature. For example, you can schedule when the DLLR object is enabled or disabled, and when the feature switches from Monitor Only mode to Shed mode. You also can schedule which target is currently active. Weekly, holiday, and exception scheduling are supported.