Local Controller Display Configuration - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document type
Technical Bulletin
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

The Local Controller Display is configured with CCT. Configure the display after selecting the hardware (NCE with Display, or FEC with Display).

With CCT you can customize many items for the display, such as how points are viewed and whether access to the display is password protected. These options are available in CCT from the Tools > Configure Displayselection while in Configuration mode. For details, refer to CCT Help.