Local Controller Display Operation Overview - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

The Local Controller Display uses a fixed set of display pages to organize the objects and data defined in the controller. Use the keys on the keypad to log on to the device and navigate between and within each page. You cannot change the order of the pages, but you can change the contents of the pages when you configure the display with CCT.