Local Controller Display Pages - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

When the controller is powered on, the screen displays a series of pages that sequence automatically to indicate the status of the controller. These pages include:

  • Diagnostic Pages – provide status information during powerup. Presents four screens that feature the Johnson Controls logo (Figure 1).

  • Controller Information Page – displays information about the controller (Figure 1).

  • Idle/Favorites Page – displays important values and frequently referenced input and output points (Figure 1).