Idle Favorites Page - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document type
Technical Bulletin
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

The Idle/Favorites page is the default view for the controller. It shows a user-defined, ordered list of points selected from within the application running in the controller (Figure 1). Use CCT to specify which objects appear on this page.

Figure 1. Idle/Favorites Page

When more than four points are configured for the Idle page, the points list scrolls vertically down the page one line at a time. You can scroll the page one item at a time by using the Up and Down Arrow keys or scroll the page four items at a time by using the Left and Right Arrow keys. Each point appears in a single row and contains its name, value, and status. The point’s status is indicated by a symbol to the left of its name (Table 1). The value of the point is updated within 5 seconds of its change.

Table 1. Icons Used for Displaying Point Status

Symbol

Description of Point Status

<none>

Point is in a normal state; no overrides.

?

Offline – Point is offline or unreliable. Actual value is unknown for offline.

*

Overridden – Point is in an overridden state.

¤

Out Of Service – Point is currently out of service.

!

Alarm - Point is currently in alarm

Note: This icon will only display for points configured with BACnet Intrinsic Alarming that are in Alarm. The icon will not display for points configured with a JCI alarm extension that are in Alarm. JCI alarm extensions are defined at the engine, and therefore will not display on the DIS17.

The Idle/Favorites page reappears whenever you log off the display or the idle timeout period expires. Pressing the Esc key when the Idle/Favorites page is displayed allows you to log on, or if already logged on, to access the Main Menu.