When the controller is turned on, the screen sequences through four
pages, as shown in Figure 1. If a
problem is detected during startup, the screen indicates the error condition. If the
controller is missing an application, the Johnson Controls screen remains with the
message Application Download Required. If an application is present, the startup
sequence completes and the Controller Information page appears (Figure 1).
Figure 1. Diagnostic Pages That Appear During Startup