Data Refresh Rate - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

Data shown on the Local Controller Display is periodically refreshed. For monitored points, the refresh rate of the Present Value and Reliability attributes is once every 5 seconds. For all other attributes, the refresh rate is within 120 seconds. After 10 minutes with no keypad activity, the refresh rate of all attributes, including Present Value and Reliability, reverts to 120 seconds.