Controller Information Page - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

The Controller Information page displays general information about the controller, such as its device name and firmware version (Figure 1). This page appears for about 8 seconds, then the Idle/Favorites Page appears (Figure 1). If the controller has not yet been commissioned by CCT, the display remains on the Controller Information page.

Figure 1. Controller Information Page - FEC Example

You can also access the information shown in Figure 1 in the attribute view format by selecting Controller Information from the Main Menu. The information shown on the Controller Information page cannot be customized.