Setting the Display Contrast - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document type
Technical Bulletin
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To set the display contrast:

Procedure

  1. Go to the Main Menu.
  2. Scroll down and select the Controller Information option.
  3. Scroll down and select the Display Contrast parameter.
  4. On the Modify page, use the Up/Down Arrow keys to select a percentage for the display contrast. The screen changes as you select a percentage.
    Figure 1. Modify Display Contrast Page

  5. Press Enter to highlight Accept. Press Enter again to save the setting.