Setting the Backlight Timeout - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document type
Technical Bulletin
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To set the backlight timeout:

Procedure

  1. Go to the Main Menu.
  2. Scroll down and select the Display Information option.
  3. Scroll down and select the Backlight Timeout parameter.
  4. On the Modify page, use the Up/Down Arrow keys to select a backlight timeout.
    Figure 1. Modify Backlight Timeout Page

  5. Press Enter to highlight Accept. Press Enter again to save the setting.