Selecting the Display Precision Style - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document type
Technical Bulletin
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To select the display precision style:

Procedure

  1. Go to the Main Menu.
  2. Scroll down and select the Display Information option.
  3. Scroll down and select the Disp (Display) Precision Style parameter.
  4. On the Modify page, use the Up/Down Arrow keys to select the style to use as the separator in a number.
    Figure 1. Modify Display Precision Style Page

  5. Press Enter to highlight Accept. Press Enter again to save the setting.