Logging Off the Display - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document type
Technical Bulletin
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To log off the display:

Procedure

  1. Go to the Main Menu.
  2. Scroll down and select the Log Off option.
  3. Press Enter. You are logged off and the Idle/Favorites page appears.
    Note: You may also log off by pressing the Esc and Enter keys at the same time.