Entering a Password - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document type
Technical Bulletin
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To enter a password:
Note: The password entry page is available only if a password was enabled when the Display Configuration was set with CCT. Otherwise, the display menus are accessible without a password entry.

Procedure

  1. Press the Escape or Enter key. The Password page appears.
    Figure 1. Password Entry Page

  2. Use the Arrow keys to select each character of your password, and press Enter to submit each character. Your entries appear in the upper right corner as asterisks. To correct an entry, use Backspace to erase one entry at a time, or press Escape to clear the entire password and start over.
  3. When you have entered the entire password, select Accept and press Enter. The password is verified and the Main Menu appears.