Displaying Overridden Points - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To display overridden points:

Procedure

  1. Go to the Main Menu.
  2. Select the Overrides option. A list of all points that are currently in override appears (Figure 1). If no points are in override, the user message Status: No objects are overridden appears.
    Figure 1. Overrides Page

  3. Use the Up/Down Arrow keys to scroll through the list of points and their current values.
  4. To display the focus page for a particular point, select the point and press Enter. The focus page for the point appears, which also allows you to command the point (for example, Release the override). Figure 2 is an example for a zone setpoint in override.
    Figure 2. Zone Setpoint Page

  5. Use the Up and Down Arrow keys to navigate through the information.