About this task
To display overridden points:
Procedure
- Go to the Main Menu.
-
Select the Overrides option. A list of all points that are currently in
override appears (Figure 1). If no points are in override,
the user message Status: No objects are overridden appears.
Figure 1. Overrides Page
- Use the Up/Down Arrow keys to scroll through the list of points and their current values.
-
To display the focus page for a particular point, select the point and press
Enter. The focus page for the point appears, which also allows you to
command the point (for example, Release the override). Figure 2 is an example for a zone
setpoint in override.
Figure 2. Zone Setpoint Page
- Use the Up and Down Arrow keys to navigate through the information.