Displaying Controller Information - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

To display controller information:

  1. Go to the Main Menu.
  2. Scroll down and select the Controller Information option.

  3. Scroll down to view each line of controller information. Table 1 lists the type of information available. None of these attributes can be modified from the display, but some are defined when the application is configured using CCT.

Table 1. Controller Display Attributes

Attribute

Description

Example

Status

Current status of the controller

Operational

CTRL

List of the controller’s point capacities

6 UI, 2 BI, 3 BO, 2 AO, 4 CO

Model Name

Model name of the controller

MS-FEC2611-0

Object Name

Object name of the controller

FC-22

System Name

Name of the system application in the controller

FCapp

Local Site Director

Name of the site director for this field controller

NAE00108d00c903

Firmware Version

Version of the firmware stored in the controller

5.1

CPU Usage

Number representing the current Central Processing Unit (CPU) usage in percent

6

FCB Mac Address

Number representing the MAC address assigned to the controller

10

FCB Baud Rate

Baud rate configured for communication on the MS/TP Bus

Auto

Note:
  • No attribute label called Status is shown; only the current status of the controller is indicated.
  • The Object Name and System Name are defined when the application is configured using CCT.
  • When a site director is not defined or is not online, this field contains four asterisks (****)