Displaying Configured Parameters and Setpoints - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document type
Technical Bulletin
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To display configured parameters and setpoints:

Procedure

  1. Go to the Main Menu.
  2. Select the Parameter/Setpoints option. A list of all configured parameters and setpoints appears.
    Figure 1. Parameter/Setpoint Page

  3. Use the Up/Down Arrow keys to scroll through the list with the current values.
  4. To get more information on a particular item, select the item and press Enter. The focus page for the item appears. Figure 2 is an example for the Occupancy Schedule.
    Figure 2. Occupancy Schedule Page

  5. Use the Up and Down Arrow keys to navigate through the information.