Displaying Configured Input and Output Points - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To display configured input and output points:

Procedure

  1. Go to the Main Menu.
  2. Select the Input/Output option. A list of all configured input and output points appears.
    Figure 1. Input/Output Page

  3. Use the Up/Down Arrow keys to scroll through the list of points and their current values.
  4. To get more information on a particular point, select the point and press Enter. The focus page for the point appears. Figure 2 is an example of a zone setpoint.
    Figure 2. Example of Zone Setpoint Page

  5. Use the Up and Down Arrow keys to navigate through the information.