Configuring the Local Controller Display with CCT - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document type
Technical Bulletin
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

NCE and FEC controllers with a display, or controllers with the remote stand-alone display, are configured with CCT. The CCT provides a Configure Display menu option that allows you to:

  • define which points appear on the display pages (Input/Output View, Parameter/Setpoint View, and Idle View) and in which order

  • define which points are read only (cannot be commanded using the display)

  • specify point names and descriptions

  • set display attributes including contrast and backlight intensity

  • select timeout settings

  • select authorization including password definition

After configuring the display, you can download the application to the controller with CCT. The changes then become effective. For details, refer to CCT Help.