Commanding Configured Parameters and Setpoints - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To command configured parameters and setpoints:

Procedure

  1. Go to the Main Menu.
  2. Select the Parameter/Setpoints option. A list of all configured parameters and setpoints appears.
  3. Use the Up/Down Arrow keys to highlight the parameter or setpoint that you want to command. Press Enter. The focus page for the item appears with the Command option highlighted.
  4. Press Enter to display the commands available to this parameter or setpoint. Figure 1 shows an example for the Command Pages.
    Figure 1. Command Page

  5. Select a Command and press Enter. An Adjust page appears. For analog points, use the Left and Right Arrow keys to position the cursor to a desired digit location; then use the Up and Down Arrow keys to increment and decrement a value. For binary points, use the Up and Down Arrow keys to scroll through the available selections. Figure 2 shows an example for the Adjust Pages.
    Figure 2. Adjust Page

  6. Press Enter to highlight Accept. Press Enter again to verify and send the command.