About this task
To command configured parameters and setpoints:
Procedure
- Go to the Main Menu.
- Select the Parameter/Setpoints option. A list of all configured parameters and setpoints appears.
- Use the Up/Down Arrow keys to highlight the parameter or setpoint that you want to command. Press Enter. The focus page for the item appears with the Command option highlighted.
-
Press Enter to display the commands available to this parameter or
setpoint. Figure 1 shows an example for the Command
Pages.
Figure 1. Command Page
-
Select a Command and press Enter. An Adjust page appears. For analog
points, use the Left and Right Arrow keys to position the cursor to a desired
digit location; then use the Up and Down Arrow keys to increment and decrement a
value. For binary points, use the Up and Down Arrow keys to scroll through the
available selections. Figure 2 shows an example for the Adjust
Pages.
Figure 2. Adjust Page
- Press Enter to highlight Accept. Press Enter again to verify and send the command.