Commanding Configured Input and Output Points - Metasys - LIT-12011270 - MS-DIS1710-0 - Field Device - DIS1710 Local Controller Display - 6

DIS1710 Local Controller Display Technical Bulletin

Product
Controls > Control Displays > DIS1710 Local Controller Display
Document number
LIT-12011270
Version
6
Revision date
2019-09-30

About this task

To command configured input and output points:

Procedure

  1. Go to the Main Menu.
  2. Select the Input/Output option. A list of all configured input and output points appears.
  3. Highlight the point that you want to command. Press Enter. The Command option for the point is highlighted.
  4. Press Enter to display the commands available to this point. Figure 1 shows an example for an analog point.
    Figure 1. Command Page

  5. Select a Command and press Enter. An Adjust page is displayed. For analog points, use the Left and Right Arrow keys to position the cursor to a desired digit location; then use the Up and Down Arrow keys to increment and decrement a value. For binary points, use the Up and Down Arrow keys to scroll through the available selections. Figure 2 shows an example for adjusting an analog setpoint.
    Figure 2. Adjust Page

  6. Press Enter to highlight Accept. Press Enter again to verify and send the command.