About this task
To command configured input and output points:
Procedure
- Go to the Main Menu.
- Select the Input/Output option. A list of all configured input and output points appears.
- Highlight the point that you want to command. Press Enter. The Command option for the point is highlighted.
-
Press Enter to display the commands available to this point. Figure 1 shows an example for an analog
point.
Figure 1. Command Page
-
Select a Command and press Enter. An Adjust page is displayed. For
analog points, use the Left and Right Arrow keys to position the cursor to a
desired digit location; then use the Up and Down Arrow keys to increment and
decrement a value. For binary points, use the Up and Down Arrow keys to scroll
through the available selections. Figure 2 shows an example for adjusting an
analog setpoint.
Figure 2. Adjust Page
- Press Enter to highlight Accept. Press Enter again to verify and send the command.