|
Field |
Description |
|---|---|
|
Connection Screen |
|
|
Connection Type |
Use to specify the connection type to use:
|
|
Connection Parameters |
Supervisor Passthru: Use to specify the following:
Note: The
Supervisor Passthru fields allows you to connect directly to a site by entering in
the site's user name and password.
Bluetooth: Use to specify the COM port and baud rate to use. MAP 4.2+ / BACnet Router: Use to specify the following:
When you first open the wizard, the default connection parameters for connecting to a MAP Gateway at version 4.2 are automatically displayed. If the connection parameters are modified, the values are stored in the wizard for future use. To restore the connection parameters to the default values, click the MAP 4.2 Default button.
Note: For further information about the MAP and common troubleshooting issues, refer to the Mobile Access Portal Gateway User's Guide (LIT-12011999).
ZigBee: Use to specify the Personal Area Network (PAN) Offset. |
|
Controller Upgrade Screen |
|
|
Browse Button |
Use to select the directory and file name of the transfer template file. |
|
Save Button |
Prompts you to browse for a directory and type a file name to save the transfer template file. |
|
Directory to Save Files to Computer Text Box and Browse Button |
Use to browse to and select the desired directory in which to transfer to the device CAFs. The selected directory appears in the field. |
|
Devices Table |
Available devices, including:
|
|
View Status Button |
Opens the Status dialog box showing the current status of the operation. Click Refresh periodically to update the status. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad. |
|
View Log Button |
Opens the Log dialog box showing the detailed operation log file. Click Refresh periodically to update the log. Click Copy To Clipboard to copy and paste the text to another word-processing program, such as Microsoft Notepad. |
|
Clear Log Button |
Clears all contents of the log file. |
|
Get Device Info Button |
Use for devices imported from a transfer template (the transfer template does not store the device model or the Boot and Main Code versions). The Get Device Info button retrieves the boot and Main Code values from the actual device so an upgrade can be properly done. |
|
Discovery Button |
Starts the Discovery process for locating devices. |
|
Stop Button |
Stops the Discovery process. |
|
Navigation Buttons |
|
|
Previous |
|
|
Clear Log Button |
Clears all contents of the log file. |
|
Get Device Info Button |
Use for devices imported from a transfer template (the transfer template does not store the device model or the Boot and Main Code versions). The Get Device Info button retrieves the boot and Main Code values from the actual device so an upgrade can be properly done. |
|
Discovery Button |
Starts the Discovery process for locating devices. |
|
Stop Button |
Stops the Discovery process. |
|
Navigation Buttons |
|
|
Previous |
|
|
Next |
Moves to the next screen of the wizard. |
|
Finish/Done |
Finish starts the transfer to device. Done appears after the transfer to device completes. Click Done to close the wizard. |
|
Cancel |
Closes the wizard without performing the transfer. |
|
|
Opens the Help system. |