Trunk Utilities - Manage Attribute Template Tool - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18
Table 1. Trunk Utilities - Manage Attribute Template Tool

Field

Description

Attribute Template Screen

Browse Button

Use to select the directory and file name of the attribute template file.

Save Button

Prompts you to browse for a directory and type a file name to save the attribute template file.

Devices Table

Available devices, including:
  • Add Device (+): Adds new device to the list.
  • Remove Device (-): Removes selected device from list.
  • Discovered Check Box: Indicates if the device is added due to device discovery (selected box) or added manually (empty box).
  • Device Name: Editable name of the device.
  • Device Address: MS/TP device address.
  • Instance Number: BACnet ID of the device.
    Note: If more than one device has the same Instance Number, the numbers display red in the device list.
  • Selected: Indicates if the device is selected (selected box) or not selected (empty box).
  • Click To Define New Attribute: Opens a tree representation of the application allowing you to select parameters to add to the template file.

Close

Closes the wizard.

Opens the Help system.