Manage Host Name and IP Address List Dialog Box - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Manage Host Name and IP Address List dialog box allows you to enter descriptions for and save multiple host names and IP addresses. These entries then appear in the drop-down box next to the Host Name/IP Address parameter.

Table 1. Manage Host Name/IP Address List Dialog Box
Field Description
Description Use to enter a description for the host name or IP address.
Host Name/IP Address Host name or IP address and allows you to edit the entry.
+ / - Adds or removes host names or IP addresses.
OK Saves the selections and closes the dialog box.
Cancel Closes the dialog box without saving.

Opens the Help system.