Transfer Controller CAFs to Computer Trunk Utility - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The Transfer Controller CAFs to Computer Trunk Utility allows you to transfer CAFs from multiple devices on the same trunk to your computer. Access this utility from the Tools menu by selecting Trunk Utilities > Transfer Controller CAFs to Computer.

After you select the devices and the directory in which to save the CAFs, the utility transfers the CAFs from the devices to the computer directory.

During the transfer to computer process, you can use the View Log and View Status options to see the transfer progress.

See the Transfer Controller CAFs to Computer steps and Trunk Utilities - Transfer Controller CAFs to Computer Wizard screens sections for information on the Transfer Controller CAFs to Computer Trunk Utility and how to use it.