Sensors (VAV-SD Subordinate) - Johnson Controls - Metasys - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document type
User Guide
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection options for the Sensors/Inputs are:

  • Supply Air Temperature: This option provides an input for stand-alone morning warm-up logic.

  • Discharge Air Temperature: This option is used primarily as a commissioning check-out feature for applications that have Box Heating to ensure the Discharge Air Temperature increases when Box Heating is commanded on.