Sensors (VAV-DD Subordinate) - Metasys - Johnson Controls - LIT-12011147 - Software Application - Controller Configuration Tool - 15.0

Controller Tool Help

Product
Controls > Control Tools > Controller Configuration Tool
Document number
LIT-12011147
Version
15.0
Revision date
2022-11-18

The selection option for Sensors/Inputs is:

  • Discharge Air Temperature: This option is used primarily as a monitoring feature during commissioning.